AXIS#.HOME.SET

Description

AXIS#.HOME.SET immediately makes the current position the home position. After using AXIS#.HOME.SET the axis command and feedback will match AXIS#.HOME.P. AXIS#.HOME.SET can be used when the axis enabled or disabled and in torque, velocity or position OpModes (AXIS#.OPMODE). If the axis is in motion when AXIS#.HOME.SET is used, the motion will be stopped and the home position set. Once the home position has been set, the addition move defined by AXIS#.HOME.DIST is not made.

Versions

Action Version Notes
Implemented 02-00-00-000
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
AXIS1.HOME.SET

6111

17DF

Unsigned8

Read/Write

-

AXIS2.HOME.SET

71647

117D

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.SET

6111

Unsigned8

Read/Write

-